- English
- German
- French
- Spanish
- Japanese
- Italian
- Chinese
- Chinese (traditional)
- Home
- Blog
- Case Study
- Knowledge Center
- Glossary
- Story
- Video
- Blog Type
- Product
- Topic
- Region
Hot Search
- Product Updates
- Share FS
- PoE Switch
- Networking
- Networking Devices
- Home
- Blog
- Case Study
- Knowledge Center
- Glossary
- Story
- Video
-
- Home
- Blog
- Case Study
- Knowledge Center
- Glossary
- Story
- Video
- Blog Type
- Product
- Topic
- Region
- Home
- Blog
- Case Study
- Knowledge Center
- Glossary
- Story
- Video
- English
Hot Search
- Product Updates
- Share FS
- PoE Switch
- Networking
- Networking Devices
Single-Mode Fiber Deployment for Data Center Excellence
As the digital landscape rapidly expands, data centers play an increasingly critical role in enterprise networks. Selecting the appropriate cabling method is crucial for ensuring the smooth operation of the data center. This article aims to explore the utilization of single-mode fiber in data centers and assist you in making a suitable selection for data center cabling.
The Rise of Single-Mode Fiber for Data Centers
Long-Distance Transmission
In modern large-scale data centers, it is common for servers, switches, and other network equipment to be positioned at distances from one another. For example, the deployment of spine-leaf cabling goes beyond having a leaf switch in a cabinet adjacent to a spine switch. The spine and leaf may be separated by hundreds of meters. In such scenarios, using a long-distance solution like single-mode optical fiber offers significant advantages.
Why is this being said? This is due to the small optical core diameter of single-mode fiber (usually 9μm), which minimizes the attenuation of optical signal intensity and enables long-distance transmission. For instance, OS2 optical fiber can support distances of up to 10km when used with an SFP+ transceiver and an LC duplex connector. Compared with single-mode, multimode is more suitable for short-distance transmission. OM4 fiber, a type of multimode, is capable of supporting 10G transmissions over a distance of 400 meters and 40/100G transmissions over a distance of 150 meters, depending on the transceiver utilized.
The table below shows the transmission distance of single-mode and multimode fiber optic cables.
Fiber Optic Cable Type
|
Fiber Cable Distance
|
||||
---|---|---|---|---|---|
Core Cladding (um)
|
1G Ethernet 1000BASE-SX
|
10G Base SE-SR
|
100G Base SR10
|
||
Multimode
|
OM1
|
62.5/125
|
275m
|
/ | / |
OM2
|
50/125
|
550m
|
/ | / | |
OM3
|
50/125
|
550m
|
300m
|
100m
|
|
OM4
|
50/125
|
550m
|
400m
|
150m
|
|
OM5
|
50/125
|
550m
|
300m
|
150m
|
|
Singlemode
|
OS1/OS2
|
9/125
|
5km
|
10km
|
/ |
Improved Bend Radius
Single-mode fiber optic cables possess a smaller bending radius. This characteristic makes them well-suited for applications that require tight bends or limited installation space.
G.652.D specifies the standard bend radius for single-mode patch cables, which is set at 30 millimeters. In contrast, the latest OS adheres to the G.657.A1 standard, which specifies a bending radius of 10mm. This smaller bending radius is three times smaller than the G.652 standard, making it highly suitable for space-constrained environments, particularly in densely cabled areas within fiber optic data centers.
Extended Lifespan
One major advantage of single-mode is its longevity: there are simply fewer generations of fiber to deal with.
For example, the OS2 optical fiber you installed 10 years ago could support a new 100 Gb/s network, such as 100GBASE-DR at 500 meters. The connectors may need replacing, but you would not need to replace new cables during tech refreshes. With multimode, an OM1 or OM2 would not be able to support a new 100GBASE-SR4 network, OM3 could only support SR4 at 70 meters, and OM4/OM5 at 100 meters.
Moreover, single-mode fiber cable has a higher channel insertion loss budget, typically ranging from 3 dB to 4 dB, compared to 1.9 dB in multimode fiber. This higher channel insertion loss budget enables the addition of more fiber adapters to the link, providing data center fibers with increased network design flexibility.
Low Signal Loss
Single-mode fiber exhibits lower signal attenuation, resulting in the preservation of data transmitted over the fiber optic cables and ensuring reliable and high-quality communication. The smaller diameter of the optical core in single-mode fiber optic cable enables a more concentrated beam, minimizing inter-mode interference that is commonly found in multi-mode fiber. As a result, data transmitted over single-mode optical fiber is more secure, reliable, and less susceptible to eavesdropping or interference.
Considerations for Data Center Cabling
-
Scalability: As data volumes continue to grow, it is essential to plan for future expansion. By designing a scalable cabling system, data center fibers can easily accommodate future growth without disruptions. Single-mode cabling provides excellent scalability because it can handle higher data rates while transmitting over long distances.
-
Security: Data center security is crucial for businesses dependent on uninterrupted data availability. When designing a cabling system, it's essential to consider the security requirements. Single-mode fibers, with their smaller core diameter compared to multimode fibers, significantly increase the difficulty for potential eavesdroppers to decipher transmitted data.
FS.COM also provides a Data Center Cabling Guide for your reference.
Conclusion
Single-mode optical cable has emerged as the attractive choice for fiber optic data centers due to its capacity to transmit signals over long distances, its flexibility in confined spaces, and its minimal signal loss. Considering these factors, data center managers can build future-proof cabling systems. However, the research and decision-making involved can be overwhelming. As a fiber data center manager, you don't have to face this challenge alone. FS.COM offers solutions and expertise to support you in making well-informed decisions.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023